JAJSFN6G September 2009 – June 2018 TCA8418
PRODUCTION DATA.
The TCA8418 provides the capability of deasserting the interrupt for 50 μs while there is a pending event. When the INT_CFG bit in Register 0x01 is set, any attempt to clear the interrupt bit while the interrupt pin is already asserted results in a 50 μs deassertion. When the INT_CFG bit is cleared, INT remains asserted if the host tries to clear the interrupt. This feature is particularly useful for software development and edge triggering applications.