4 改訂履歴
Changes from B Revision (May 2018) to C Revision
- Changed VCC = 1.65 V to 5.5 V To: VCC = 2.5 V in Figure 15Go
Changes from A Revision (May 2014) to B Revision
- 「概要」の最初の段落を変更Go
- Added Tstg to the Absolute Maximum Ratings tableGo
- Changed the first paragraph of the Overview sectionGo
- Changed "switch" to "multiplexer" in the Feature Description sectionGo
- Changed text in the Control Register Definition section From: "One or several SCn/SDn downstream pairs, or channels, are selected..." To: "One SCn/SDn downstream pair, or channel, is selected..."Go
Changes from * Revision (May 2014) to A Revision