JAJSI81B April 2014 – November 2019 TCA9546A
PRODUCTION DATA.
A typical application of the TCA9546A contains anywhere from 1 to 5 separate data pull-up voltages, VDPUX , one for the master device (VDPUM) and one for each of the selectable slave channels (VDPU0 – VDPU3). In the event where the master device and all slave devices operate at the same voltage, then the pass voltage, Vpass = VDPUX. Once the maximum Vpass is known, Vcc can be selected easily using Figure 16. In an application where voltage translation is necessary, additional design requirements must be considered (See Design Requirements).
Figure 15 shows an application in which the TCA9546A can be used.