JAJSI81B April 2014 – November 2019 TCA9546A
PRODUCTION DATA.
In the event of a glitch or data corruption, TCA9546A can be reset to its default conditions by using the power-on reset feature. Power-on reset requires that the device go through a power cycle to be completely reset. This reset also happens when the device is powered on for the first time in an application.
A power-on reset is shown in Figure 19.
Table 2 specifies the performance of the power-on reset feature for TCA9546A for both types of power-on reset.
PARAMETER | MIN | TYP | MAX | UNIT | ||
---|---|---|---|---|---|---|
VCC_FT | Fall time | See Figure 19 | 1 | 100 | ms | |
VCC_RT | Rise time | See Figure 19 | 0.1 | 100 | ms | |
VCC_TRR | Time to re-ramp (when VCC drops below VPORF(min) – 50 mV or when VCC drops to GND) | See Figure 19 | 40 | μs | ||
VCC_GH | Level that VCC can glitch down to, but not cause a functional disruption when VCC_GW = 1 μs | See Figure 20 | 1.2 | V | ||
VCC_GW | Glitch width that will not cause a functional disruption when VCC_GH = 0.5 × VCC | See Figure 20 | 10 | μs | ||
VPORF | Voltage trip point of POR on falling VCC | See Figure 21 | 0.8 | 1.25 | V | |
VPORR | Voltage trip point of POR on rising VCC | See Figure 21 | 1.05 | 1.5 | V |
Glitches in the power supply can also affect the power-on reset performance of this device. The glitch width (VCC_GW) and height (VCC_GH) are dependent on each other. The bypass capacitance, source impedance, and device impedance are factors that affect power-on reset performance. Figure 20 and Table 2 provide more information on how to measure these specifications.
VPOR is critical to the power-on reset. VPOR is the voltage level at which the reset condition is released and all the registers and the I2C/SMBus state machine are initialized to their default states. The value of VPOR differs based on the VCC being lowered to or from 0. Figure 21 and Table 2 provide more details on this specification.