JAJSGL8E December 2014 – October 2024 TCA9617B
PRODUCTION DATA
Multiple TCA9617Bs can be connected in series as long as the A side is connected to the B side. I2C bus target devices can be connected to any of the bus segments. The number of devices that can be connected in series is limited by repeater delay/time-of-flight considerations on the maximum bus speed requirements.