JAJSL28E january 2021 – march 2023 TCAN1043A-Q1
PRODUCTION DATA
nFAULT is a logic-level output signal, referenced to VIO, from the TCAN1043A-Q1 to a CAN FD controller. The nFAULT output is driven to the VIO level as logic-high output.
The nFAULT output is used to transmit the TCAN1043A-Q1 status indicator flags to the CAN FD controller. Please see Table 8-1 for the specific fault scenarios that are indicated externally via the nFAULT pin. The TCAN1043A-Q1 puts the nFAULT pin in the high-impedance state in the Sleep mode to conserve power because there are no fault scenarios that are indicated externally in the Sleep mode.