JAJSNX3 February 2024 TCAN1465-Q1 , TCAN1469-Q1
ADVANCE INFORMATION
The INH pin is a high voltage output pin that provides voltage from the VSUP minus a diode drop to enable an external high voltage regulator. These regulators are usually used to support the microprocessor and VIO pin. The INH function is on in all modes except for sleep mode. In sleep mode the INH pin is turned off, going into a high Z state. This allows the node to be placed into the lowest power state while in sleep mode. If this function is not required it can be disabled by setting register 8'h1A[6] = 1b using the SPI interface. The TCAN1469-Q1 can configure this pin as a LIMP home pin by setting register 8'h1A[5] = 1b. When configured as the LIMP pin it is connected to external circuitry for a limp home mode. If a Watchdog fault occurs, exceeding the programmed watchdog error counter, the device turns on the LIMP pin. If Fail-safe mode is enabled, the LIMP pin will turn on when entering this mode. Once on, the LIMP pin will be on until the programmed watchdog error free behavior requirement is met according to LIMP_SEL_RESET at register 8'h1A[3:2]. Writing a 1b to 8'h1A[1], LIMP_RESET, will turn off the LIMP pin.