JAJSNX3 February 2024 TCAN1465-Q1 , TCAN1469-Q1
ADVANCE INFORMATION
If VIO drops below UVIO under-voltage detection several functions are disabled. The transceiver switches off and disengages from the bus until VIO has recovered. When UVIO triggers, the tUV timer starts. If the timer times out and the UVIO is still there, the device enters sleep mode. See Figure 8-10, Figure 8-11. Once in sleep mode, a wake event is required to place the TCAN146x-Q1 into standby mode and enable the INH pin. As registers are cleared in sleep mode, the UVIO interrupt flag is lost. If the UVIO event is still in place, the cycle repeats. If during a thermal shut down event a UVIO event happens, the device automatically enters sleep mode. See Figure 8-25 on how UVIO behaves.
The device is designed to be passive or no load to the CAN bus if the device is unpowered. The bus terminals (CANH, CANL) have low leakage currents when the device is unpowered not loading the bus. This is critical if some nodes of the network are unpowered while the rest of the of network remains operational. Logic terminals also have low leakage currents when the device is unpowered, which avoids loading other circuits which can remain powered.
The UVLO circuit monitors both rising and falling edge of a power rail when ramping and declining.