JAJSVM2 November 2024 TDP142-Q1
ADVANCE INFORMATION
The purpose of receiver equalization is to compensate for channel insertion loss and inter-symbol interference in the system before the input of the TDP142-Q1. The receiver overcomes these losses by attenuating the low-frequency components of the signals with respect to the high-frequency components. Select the proper gain setting to match the channel insertion loss before the input of the TDP142-Q1 receivers. Two 4-level inputs pins enable up to 16 possible equalization settings. The TDP142-Q1 also provides the flexibility of adjusting settings through I2C registers.