JAJSHX3 September 2019 THVD1505
PRODUCTION DATA.
THVD1505 polarity correction can also work without a fail-safe resistor network. See Figure 20.
In this scenario, the master node drives the bus for longer than tFS. After a time, t > tFS, the master begins transmitting data. Figure 21 shows the timing diagram for active polarity definition. DIR pin refers to the output of the MCU that is driving DE and RE pins in Figure 21.
POLCOR logic behavior with active polarity definition is identical to the POLCOR logic behavior with passive polarity definition.