JAJSIJ1G October 2009 – August 2023 TL331-Q1 , TL331B-Q1 , TL391B-Q1
PRODMIX
Output current is determined by the load/pull-up resistance and logic/pull-up voltage. The output current will produce a output low voltage (VOL) from the comparator. In which VOL is proportional to the output current. Use Figure 6-3 to determine VOL based on the output current.
The output current can also effect the transient response. More is explained in the next section.