JAJSO93A May 2022 – December 2022 TLIN1431-Q1
PRODUCTION DATA
デバイスごとのパッケージ図は、PDF版データシートをご参照ください。
This pin determines if the TLIN1431x-Q1 watchdog and mode changes are controlled by pin or SPI. At power up, the device monitors this pin and determine which method is to be used. When tied to GND, the device is pin programmable, see Figure 8-5. When connected to a high-Z processor IO pin or pulled up, the device is set up to support SPI, see Figure 8-6. In SPI control mode, if the LDO is being used to power up circuitry other than the processor a mismatch can take place. An example of this is using the TLIN14315-Q1 VCC to power up a 5 V sensor and the processor supports 3.3 V IO electrical levels. This is accomplished by letting the PIN/nCS pin float at power up which configures the internal IO electrical levels to VINT which is 3.3 V. For the IO to be 5 V, an external 500 kΩ resistor needs to be pulled up to the 5 V VCC pin. This makes the IO 5 V. See Figure 8-4 to understand the three ways this pin can be connected for the 5 V LDO device.
The behavior of the microprocessor used must be understood if connecting to this pin to control whether the device is to be pin controlled or SPI controlled. There is an internal pull-up that sets the device in SPI control mode. If the processor pin drives low during power up, the device is in pin control mode. To specify pin control mode place and external pull-down resister to ground.