JAJSL93B March 2021 – February 2024 TLIN2029A-Q1
PRODUCTION DATA
The RXD output structure is an open-drain output stage. This allows the TLIN2029A-Q1 to be used with 3.3V and 5V I/O processor. If the RXD pin of the processor does not have an integrated pull-up, an external pull-up resistor to the processor I/O supply voltage is required. The select external pull-up resistor value should be between 1kΩ to 10kΩ, depending on supply used (See IOL in Electrical Characteristics). The VSUP pin of the device should be decoupled with a 100nF capacitor by placing it close to the VSUP supply pin. The system should include additional decoupling on the VSUP line as needed per the application requirements.