SNOSDG0 August 2024 TLV1H103-SEP
PRODUCTION DATA
The TLV1H103-SEP has two modes of operation. The first is an active mode where the output reflects the condition at the inputs when an external resistor is connected to ground on the LE/HYS pin. The resistor value creates a specified amount of internal hysteresis for the comparator without requiring external, positive feedback. The second is a latch mode where the output is held at the last active state when the LE/HYS pin is pulled low. The TLV1H103-SEP returns to active mode after a short delay when the pin is pulled high.