JAJSFH2C November 2017 – March 2024 TLV755P
PRODUCTION DATA
デバイスごとのパッケージ図は、PDF版データシートをご参照ください。
As with most LDOs, excessive reverse current potentially damages this device.
Reverse current flows through the body diode on the pass transistor instead of the normal conducting channel. At high magnitudes, this current flow degrades the long-term reliability of the device, as a result of one of the following conditions:
Conditions where reverse current occur are outlined in this section, all of which exceed the absolute maximum rating of VOUT > VIN + 0.3V:
If reverse current flow is expected in the application, use external protection to protect the device. Figure 7-3 shows one approach of protecting the device.