JAJSF56D April 2018 – October 2023 TLV758P
PRODUCTION DATA
Figure 7-1 shows that the output voltage of the TLV758P can be adjusted from 0.55 V to 5.5 V by using a resistor divider network.
The adjustable-version device requires external feedback divider resistors to set the output voltage. VOUT is set using the feedback divider resistors, R1 and R2, according to the following equation:
For this device, VFB = 0.55 V.
To ignore the FB pin current error term in the VOUT equation, set the feedback divider current to 100 times the FB pin current listed in the Electrical Characteristics table. This setting provides the maximum feedback divider series resistance, as shown in the following equation:
For this device, IFB = 10 nA.