JAJSJS6B June 2021 – July 2024 TMAG5273
PRODUCTION DATA
Figure 6-8 shows an example of the general call I2C write command supported by the TMAG5273. This command is useful to configure multiple I2C devices in a I2C bus simultaneously. The starting byte contains 8-bit 0s. The MSB of the second byte contains the conversion trigger bit. Write 1 at this trigger bit to start a new conversion after the register address decoding is completed. The seven LSB bits of the second byte contains the starting register address for the write command. After the two command bytes, the primary device starts to send the data to be written at the corresponding register address of all the secondary devices in the I2C bus. Each successive write byte sends the data for the successive register address in the secondary devices.