JAJSIC9A October 2015 – October 2015 TMP107-Q1
PRODUCTION DATA.
Only the host initiates communication. Before communication begins, all the daisy-chained devices are in transparent mode. In this mode, all the host operations are sequentially transferred to all the devices in the chain. The devices in the chain cannot communicate with each other with the exception of the address initialize command. After initialization, the devices in the chain are in one of the following four modes: