JAJSGF6D May 2015 – January 2020 TMP107
PRODUCTION DATA.
Use the global write operation to write data to a specific register in multiple parts. The sequence of the communication is shown in Figure 28. Data in this operation are written to the registers in all the devices from the first device to the address specified in the address field of the command and address phase.