JAJSGF6D May 2015 – January 2020 TMP107
PRODUCTION DATA.
To avoid any bus contention between the host and the TMP107 devices, use a tri-state buffer, such as the SN74LVC1G125. Use a 100-Ω resistor (typical) in series with the RX input to limit the amount of current in case of overshoot. A 10-Ω resistor (typical) between the tri-state buffer and the first TMP107 device reduces any signal collisions between the buffer and the TMP107 by limiting the amount of current flow. The pullup resistor at the output of the tri-state buffer defines the baud rate of communication. Use a 4.1-kΩ pullup resistor, as shown in Figure 39, to support the entire baud rate range specified in the Timing Requirements. A 0.1-μF bypass capacitor is recommended for each TMP107 device in the daisy-chain.