JAJSME8C July 2021 – June 2022 TMP126
PRODUCTION DATA
The ALERT pin of the TMP126 can be programmed to operate in two different modes. In the interrupt mode the TMP126 will assert the ALERT pin if the temperature exceeds the limits set by temperature limit registers and the flags are enabled. After the Alert_Status is read and the interrupt bits cleared, the ALERT pin will be de-asserted. In the Comparator mode, the ALERT pin will assert if any enabled status bits of the Alert_Status are set. Changes to the Alert_Enable register will be reflected on the ALERT pin after the completed conversion or device read.