JAJSJN1A May 2023 – September 2023 TMP4718
PRODUCTION DATA
The device includes a fault queue feature. When enable in the register settings, the ALERT and T_CRIT will only be generated if there are three consecutive temperature conversion results beyond the limits. When this feature is disabled, only one temperature conversion result beyond the limits will generate an ALERT or T_CRIT warning.
This feature only applies to the remote channel and will have no effect on the local channel. The fault queue is enabled upon device POR (that is, three successive temperature results beyond the limits triggers an ALERT or T_CRIT warning).