JAJSKO9A March 2020 – March 2021 TMUX4157N
PRODUCTION DATA
Bandwidth is defined as the range of frequencies that are attenuated by less than 3 dB when the input is applied to the source pin (Sx) of an on-channel, and the output is measured at the drain pin (D) of the device. Figure 7-11 shows the setup used to measure bandwidth.