JAJSES2A February 2018 – September 2018 TMUX6104
PRODUCTION DATA.
Break-before-make delay is a safety feature that prevents two inputs from connecting when the TMUX6104 is switching. The TMUX6104 output first breaks from the on-state switch before making the connection with the next on-state switch. The time delay between the break and the make is known as break-before-make delay. Figure 21 shows the setup used to measure break-before-make delay, denoted by the symbol tBBM.