JAJSES2A February 2018 – September 2018 TMUX6104
PRODUCTION DATA.
Bandwidth is defined as the range of frequencies that are attenuated by < 3 dB when the input is applied to the source pin (Sx) of an on-channel, and the output is measured at the drain pin (D) of the TMUX6104. Figure 26 shows the setup used to measure bandwidth of the mux. Use Equation 4 to compute the attenuation.