JAJSG83A September 2018 – December 2018 TMUX6119
PRODUCTION DATA.
AC PSRR measures the ability of a device to prevent noise and spurious signals that appear on the supply voltage pin from coupling to the output of the switch. The DC voltage on the device supply is modulated by a sine wave of 620 mVPP. The ratio of the amplitude of signal on the output to the amplitude of the modulated signal is the AC PSRR. Figure 29 shows the setup used to measure ACPSRR of the TMUX6119.