JAJSGK3A November 2018 – October 2022 TMUX6136
PRODUCTION DATA
The TMUX6136 have a simple transmission-gate topology. Any mismatch in capacitance between the NMOS and PMOS transistors results in a charge injected into the drain or source during the falling or rising edge of the gate signal. The amount of charge injected into the source of the device is known as charge injection, and is denoted by the symbol QINJ. Figure 7-6 shows the setup used to measure charge injection from drain (D) to source (Sx).