JAJSNE3B march 2022 – july 2023 TMUX7348F , TMUX7349F
PRODMIX
The TMUX7348F and TMUX7349F enters into Fault mode when any of the input signals on the source (Sx) pins exceed VFP or VFN by a threshold voltage VT. Under the overvoltage condition, the switch input experiencing the fault automatically turns OFF regardless of the logic status, and the source pin becomes high impedance with a negligible amount of leakage current flowing through the switch. When the fault channel is selected by the logic control, the drain pin (D or Dx) is pulled to the fault supply that was exceeded through a 40 kΩ internal resistor.
In the Fault mode, the general fault flag (FF) is asserted low. Table 9-1 and Table 9-2 provides how the specific flag (SF) is asserted low when a specific input path is selected.
The overvoltage protection is provided only for the source (Sx) input pins. The drain (D or Dx) pin, if used as signal input, must stay in between VFP and VFN at all time since no overvoltage protection is implemented on the drain pin.