SLOS733B January 2012 – April 2016 TPA2080D1
PRODUCTION DATA.
Place all the external components close to the TPA2080D1 device. Placing the decoupling capacitors as close as possible to the device is important for the efficiency of the class-D amplifier. Any resistance or inductance in the trace between the device and the capacitor can cause a loss in efficiency.
It is important to operate the TPA2080D1 at temperatures lower than its maximum operating temperature. The maximum ambient temperature depends on the heat-sinking ability of the PCB system. Given θJA of 97.3°C/W, the maximum allowable junction temperature of 150°C, and the internal dissipation of 0.5 W for 1.9-W, 8 Ω-load, 3.6-V supply, the maximum ambient temperature is calculated as:
The calculated maximum ambient temperature is 101.4°C at maximum power dissipation at 3.6-V supply and 8-Ω load. The TPA2080D1 is designed with thermal protection that turns the device off when the junction temperature surpasses 150°C to prevent damage to the IC.
TPA2080D1 has AGND, BGND and PGND for analog circuit, boost converter and Class-D amplifier respectively. These three ground pins should be connected together through a solid ground plane with multiple ground VIAs.
In making the pad size for the WCSP balls, it is recommended that the layout use non-solder mask defined (NSMD) land. With this method, the solder mask opening is made larger than the desired land area, and the opening size is defined by the copper pad width. Figure 25 shows the appropriate diameters for a WCSP layout.
SOLDER PAD DEFINITIONS |
COPPER PAD |
SOLDER MASK (5)
OPENING |
COPPER THICKNESS |
STENCIL (6) (7)
OPENING |
STENCIL THICKNESS |
---|---|---|---|---|---|
Nonsolder mask defined (NSMD) | 275 μm (+0.0, -25 μm) |
375 μm (+0.0, -25 μm) | 1 oz max (32 μm) | 275 μm x 275 μm Sq. (rounded corners) |
125 μm thick |