JAJSKR7B September 2019 – December 2020 TPA6304-Q1
PRODUCTION DATA
The pinout of the TPA6304-Q1 was selected to provide flow through layout with all high-power connections on the right side, and all low-power signals and supply decoupling on left side.
Section 10.2 shows the area for the components in the application example (see the Figure 8-2 section). This layout example is taken from the EVM PCB.
The TPA6304-Q1 EVM uses a four-layer PCB. The copper thickness was selected as 70 µm to optimize power loss.
The small value of the output filter provides a small size and, in this case, the low height of the inductor enables double sided mounting.