JAJSKR7B September 2019 – December 2020 TPA6304-Q1
PRODUCTION DATA
The DC load diagnostics are used to verify the load is connected properly.
In order to support fast system level start up requirements to play audio:
DC Diagnostics pass and allow a channel to enter MUTE or PLAY mode if the following tests pass on the output pins:
On completion of the diagnostic routine where no fault is reported, the respective CH(i) LDG STATE REPORT bit of Channel State Report CH1, CH2 Register or Channel State Report CH3, CH4 Register is set high.
Any of the following conditions start the DC Load Diagnostics: