JAJSJN8C January 2016 – August 2020 TPD3S714-Q1
PRODUCTION DATA
When the current through the VBUS path exceeds the ILIM current threshold, the device enters into the overcurrent state. The TPD3S714-Q1 limits current to the ILIM threshold by dropping voltage across the VBUS FET to maintain constant current. Once it continues to sense an overcurrent condition for the blanking time tBLANK, the device disables itself for the retry time, tRETRY and then retry automatically for the retry time, tBLANK_RETRY. In the event that the current is below the overcurrent threshold, the device deasserts fault and resumes normal operation.