JAJSCG6 September 2016 TPL5010-Q1
PRODUCTION DATA.
PIN | TYPE(1) | DESCRIPTION | APPLICATION INFORMATION | |
---|---|---|---|---|
NO. | NAME | |||
1 | VDD | P | Supply voltage | |
2 | GND | G | Ground | |
3 | DELAY/ M_RST | I | Time Interval set and Manual Reset | Resistance between this pin and GND is used to select the time interval. The reset switch is also connected to this pin. |
4 | DONE | I | Logic Input for watchdog functionality | Digital signal driven by the µC to indicate successful processing of the WAKE signal. |
5 | WAKE | O | Timer output signal generated every tIP period. | Digital pulsed signal to wake up the µC at the end of the programmed time interval. |
6 | RSTn | O | Reset Output (open drain output) | Digital signal to RESET the µC, pull-up resistance is required |