JAJSG91B June 2015 – September 2018 TPL5111
PRODUCTION DATA.
The time interval between two adjacent DRVn pulses (rising edges, in timer mode) is selectable through an external resistance (REXT) between the DELAY/M_DRV pin and ground. The resistance (REXT) must be in the range between 500 Ω and 170 kΩ. At least a 1% precision resistance is recommended. See Selection of the External Resistance on how to set the time interval using REXT. During start-up, the external resistance is read immediately after POR.