JAJSG91B June 2015 – September 2018 TPL5111
PRODUCTION DATA.
PIN | TYPE(1) | DESCRIPTION | APPLICATION INFORMATION | |
---|---|---|---|---|
NO. | NAME | |||
1 | VDD | P | Supply voltage | |
2 | GND | G | Ground | |
3 | DELAY/ M_DRV | I | Time interval configuration (during power on) and logic input for manual Power ON | Resistance between this pin and GND is used to select the time interval. The manual Power ON signal (logic HIGH) can also connected to this pin. |
4 | DONE | I | Logic Input for watchdog functionality | Digital signal driven by the µC to indicate successful processing. |
5 | DRVn | O | Power Gating output signal generated every tIP | The ENABLE pin of the LDO or DC-DC converter is connected to this pin. DRVn is active HIGH. |
6 | EN/ ONE_SHOT | I | Select mode of operation | When EN/ONE_SHOT = HIGH, the TPL5111 works as a TIMER. When EN/ONE_SHOT = LOW, the TPL5111 asserts DRVn one time for the programmed time interval. In this mode, the DRVn signal may be manually asserted by applying a logic HIGH to the DELAY/M_DRV pin. |