SLVSHA1 September 2024 TPS1685
ADVANCE INFORMATION
PIN | TYPE(1) | DESCRIPTION | |
---|---|---|---|
NAME | NO. | ||
ILIM | 1 | I/O | An external resistor from this pin to GND sets the active current sharing threshold during steady-state. This pin also serves as individual eFuse current monitor output during steady state. Do not leave floating. |
IMON | 2 | I/O | An external resistor from this pin to GND sets the overcurrent protection threshold and fast-trip threshold during steady-state. This pin also acts as a fast and accurate analog output load current monitor signal during steady-state. Do not leave floating. |
IREF | 3 | I/O | This pin sets the reference voltage for overcurrent, short-circuit protection and active current sharing blocks. The reference voltage can be generated using internal current source and resistor on this pin, or can be driven from external voltage source. Do not leave floating. |
dVdT | 4 | I/O | This pin is used to configure the output slew rate during Start-up. Leave this pin open to allow fastest start-up. Connect capacitor to ground to slow down the slew rate to manage inrush current. |
GND | 5 | G | Device ground reference pin. Connect to system ground. |
SFT_SEL | 6 | I/O | This pin selects the scalable fast trip threshold multiplier during steady state. Connect a resistor from this pin to GND to select the SFT multiplier. |
OUT | 7, 8 | P | Power output. Must be soldered to the output power plane uniformly for proper heat dissipation. |
VDD | 9 | P | Controller power input pin. Can be used to power the internal control circuitry with a filtered and stable supply which is not affected by system transients. Connect this pin to VIN through a series resistor and add a decoupling capacitor to GND. |
IN | 10, 22, 23 | P | Power input. Must be soldered to the input power plane uniformly for proper heat dissipation. |
NC | 11, 17, 21 | — | Do not connect anything to this pin. |
MODE | 12 | I | This pin is used to configure the device for standalone/primary or secondary mode. Connect the pin to GND to configure device as a secondary to a primary eFuse/controller. Leave the pin floating for standalone/primary mode of operation. |
FLT | 13 | O | This is an open drain active low pin which is pulled low to indicate a fault. Pull up this pin to external supply voltage with a resistor. |
ITIMER | 14 | I/O | A capacitor from this pin to GND sets the overcurrent blanking interval during which the output current can temporarily exceed the overcurrent threshold (but lower than fast-trip threshold) during steady-state operation before the device overcurrent response takes action. |
TEMP | 15 | I/O | Analog voltage output for junction temperature. Can be tied together with TEMP outputs of multiple devices in a parallel configuration to indicate the peak temperature of the parallel chain. |
EN/UVLO | 16 | I | Active high enable input. Connect resistor divider from input supply to set the undervoltage threshold. Do not leave floating. |
OVP | 18 | I | This pin can be used to set the over-voltage set-point. Connect a resistor divider from VIN to this pin. Do not leave floating. |
PGOOD | 19 | O | This is an open-drain active high power good pin which is asserted high when the device is in steady state. This pin has weak internal pull-up to internal supply voltage. |
SWEN | 20 | I/O | This is an open-drain signal to indicate and control power switch ON/OFF status. This pin facilitates active synchronization between multiple devices in a parallel chain. This pin has weak internal pull-up to internal supply voltage. |
IN | PowerPad | P | Power input. Must be soldered to the input power plane uniformly for proper heat dissipation. |