JAJSC11D October 2014 – December 2019 TPS1H100-Q1
PRODUCTION DATA.
Reverse-polarity detection has the same detection mechanism and behavior as open-load detection, both in the on-state and off-state. See the fault truth table, Table 1, for more details. In the on-state, the reverse current flows through the FET instead of the body diode, leading to less power dissipation. Thus, the worst case off-state is when reverse current occurs. In off-state, the reverse current should be lower than Irev1 to ensure the survival of the device. See Reverse Current Protection for more external protection circuitry information.