JAJSC11D October 2014 – December 2019 TPS1H100-Q1
PRODUCTION DATA.
When loss of GND occurs, output is turned off regardless of whether the input signal is high or low.
Case 1 (loss of device GND): Loss of GND protection is active when the Tab, IC_GND, and current limit GND are one trace connected to the board GND, as shown in Figure 38. Tab floating is also a choice.
Case 2 (loss of module GND): When the whole ECU module GND is lost, protections are also active. At this condition, the load GND remains connected.