JAJSER0D February 2018 – September 2021 TPS1H200A-Q1
PRODUCTION DATA
Auto-retry mode is active when the DELAY pin is externally pulled up. The pullup voltage must be higher than Vdl(th). When the current limit is reached, the output current holds at the setting current, but periodically turns on for thic(on) and turns off for thic(off). The device checks the current limit status at the falling edge of thic(on) clock. If current limit status is captured, the device shuts down for thic(off). If the current limit status is not captured because of the off window during the thermal conditions, the device keeps turning on for additional thic(on) or more until the current limit status is captured.