JAJSER0D February 2018 – September 2021 TPS1H200A-Q1
PRODUCTION DATA
Latch-off mode is active when the DELAY pin connects to GND through a capacitor. When a current limit is reached, the output current holds at the setting current, but latches off after a preset DELAY time (tdl1+ tdl2). tdl1 is the default delay time, and tdl2 is a configurable delay time set by a capacitor. Regardless of whether the current limit is removed or not, the output remains latched off. The output only recovers when IN is toggling.
tdl2 can be calculated by Equation 2.
where