JAJSJE1A July 2021 – December 2021 TPS1HC100-Q1
PRODUCTION DATA
デバイスごとのパッケージ図は、PDF版データシートをご参照ください。
A high-accuracy current limit allows higher reliability, which protects the power supply during short circuit or power up. Also, a current limit can save system costs by reducing PCB traces, connector size, and the capacity of the preceding power stage.
Current limiting offers protection from over-stressing to the load and integrated power FET. The current limit regulates the output current to the set value, and pulls up the SNS pin to VSNSFH and asserts the FLT pin as diagnostic reports. The three current-limit thresholds are:
Additionally, this value can be dynamically changed by changing the resistance on the ILIM pin. This information can be seen in the Applications section.
Both the internal current limit (Ilim,nom) and external programmable current limit are always active when VBB is powered and EN is high. The lower value one (of ILIM and the external programmable current limit) is applied as the actual current limit. The typical deglitch time for the current limit to assert is 2.5 µs.
Note that if a GND network is used (which leads to the level shift between the device GND and board GND), the ILIM pin must be connected with device GND. Calculate RILIM with Equation 2.
For better protection from a hot short condition (when VBB is high, channel is on, and a short to GND happens suddenly), an over current protection, OVCR, circuit is triggered that makes sure to limit the maximum current the device allows to go through. With this OVCR, the device is protected during hot short events.
For more information about the current limiting feature, see the Short-Circuit and Overload Protection section.
The TPS1HC100-Q1 has very tight accuracy of the current limit regulation level across the full range of currents and temperature. This accuracy is defined at several defined RILIM values, 7.15 kΩ, 25 kΩ, and 71.5 kΩ specified in the Electrical Characteristics. As the current limit is changed with the RILIM, the KCL ratio value also slightly changes. Additionally, the current limit architecture in the device allows for the tightest variation at current limit set by a 25-kΩ RILIM, 1.9 A, of +18%, -7% and at the lower and upper ends of the range, 690 mA and 6.15 A respectively, to be about ±25%. Then, using the boundaries for RILIM of 7.15 kΩ and 71.5 kΩ, a graph can be built to linearly interpret the error for RILIM values that are inside of the range. This graph can be seen in the figure below.
Using this figure, the error can be estimated for any current limit value desired, and the associated KCL value can determine the RILIM resistor appropriate. This graph does not take into account RILIM resistor tolerances, only the error associated with the current limit regulation.