JAJSN24A November 2021 – June 2022 TPS22953-Q1 , TPS22954-Q1
PRODUCTION DATA
The EN pin controls the state of the switch. When the voltage on EN exceeds VIH,EN the switch enables. When EN goes below VIL,EN the switch disables.
The EN pin has a blanking time of tBLANK on the rising edge after the VIH,EN threshold has been exceeded. The EN pin also has a de-glitch time of tDEGLITCH when the voltage has gone below VIL,EN.
The EN pin can also be configured through an external resistor divider to monitor a voltage signal for input UVLO. See Equation 1 and Figure 9-1 on how to configure the EN pin for input UVLO.
where