JAJSF19A September 2017 – December 2017 TPS23521
PRODUCTION DATA.
In this state the hot swap FET is turned off and the controller is waiting for the insertion delay to finish. This allows the input supply to settle after a Hot Plug. If any of the following occur, the controller will be kicked back to the OFF state:
Once the insertion delay is finished, the controller will move to the Start-up state.