JAJSHI3C March 2019 – October 2019 TPS23881
PRODUCTION DATA.
Upon power up, the TPS23881 device can operate from its internal ROM memory or users have the option of programming the SRAM via I2C.
NOTE
The latest version of TPS23881 firmware may be accessed from the TI mySecure Software webpage.
All I2C traffic other than those commands outlined below to program the SRAM shall be deferred until after the SRAM programming sequences below are complete.
For systems that include multiple TPS23881 devices, the 0x7F "global" broadcast I2C address may be used to programmed all of the devices at the same time.
Refer to the How to Load TPS2388x SRAM Code document on TI.com for more detailed instructions on the SRAM programing procedure.