JAJSHI3C March 2019 – October 2019 TPS23881
PRODUCTION DATA.
COMMAND = 19h with 1 Data Byte, Write Only
Push button register.
Used to initiate a channel(s) turn on or turn off in any mode except OFF mode.
7 | 6 | 5 | 4 | 3 | 2 | 1 | 0 |
POFF4 | POFF3 | POFF2 | POFF1 | PWON4 | PWON3 | PWON2 | PWON1 |
W-0 | W-0 | W-0 | W-0 | W-0 | W-0 | W-0 | W-0 |
LEGEND: R/W = Read/Write; R = Read only; W = Write only; -n = value after reset |
Bit | Field | Type | Reset | Description |
---|---|---|---|---|
7–4 | POFF4–POFF1 | W | 0 | Channel power off bits |
3–0 | PWON4–PWON1 | W | 0 | Channel power on bits |
SPACE
NOTE
Writing a “1” at POFFn and PWONn on same Channel during the same write operation turns the Channel off.
NOTE
The tOVLD, tLIM, tSTART and disconnect events have priority over the PWON command. During tOVLD, tLIM or tSTART, cool down cycle, any channel turn on using Power Enable command will be ignored and the Channel will be kept off.
NOTE
For 4-Pair wired ports:
These bits control the individual Channel response of each Channel. Thus it is recommended that for 4-pair wire ports, the bits for both channels be set simultaneously.
In Semi Auto mode with DETE = CLE = 1 on both channels, it is permissible to set only one PWON bit to attempt to turn on only that singular channel.
For 4P Single Signature devices that classify as class 5-8, a singular PWON command will fail and a STRT fault set with the “insufficient power” code written to 0x24.
If the PD presents itself as class 4 or below, then only that pair set will be powered.
Setting the alternate PWON bit for the secondary channel of a single signature device after the primary is already powered will result in the immediate turn on of the channel without completing DET or CLS.
For a 4-Pair Dual Signature device that has only one channel powered, setting the PWON bit for the unpowered channel will result in a turn on attempt on that channel based on the assigned classification of the other channel and the Power Allocation settings in 0x29h at the time of the new PWON command.
PWONn in Diagnostic/Manual Mode:
If the PSE controller is configured in Diagnostic mode, writing a “1” at that PWONn bit location will immediately turn on the associated Channel.
SPACE
PWONn in Semi Auto Mode:
While in Semi Auto mode, writing a “1” at a PWONn bit will attempt to turn on the associated Channel. If the detection or class results are invalid, the Channel is not turned on, and there will be no additional attempts to turn on the Channel until this push button is reasserted and the channel will resume its configured semi auto mode operation.
NOTE
In Semi Auto mode, the Power Allocation (0x29h) value needs to be set prior to issuing a PWON command. Any changes to the Power Allocation value after a PWON command is given may be ignored.
CLEn | DETEn | Channel Operation | Result of PWONn Command |
---|---|---|---|
0 | 0 | Idle | Singular Turn On attempted with Full DET and CLS cycle |
0 | 1 | Cycling Detection Measurements only | Singular Turn On attempted with Full DET and CLS cycle |
1 | 0 | Idle | Singular Turn On attempted with Full DET and CLS cycle |
1 | 1 | Cycling Detection and Classification Measurements | Singular Turn On attempted after next (or current) DET and CLS cycle |
In semi auto mode with DETE and CLE set, as long as the PWONx command is received prior to the start of classification, the Channel will be powered immediately after classification is complete provided the classification result is valid and the power allocations settings (see register 0x29h) are sufficient to enable power on.
SPACE
PWONn in Auto Mode:
In Auto mode with DETE or CLE set to 0, a PWONx command will initiate a singular detection and classification cycle and the port/channel will be powered immediately after classification is complete provided the classification result is valid and the power allocations settings (see register 0x29h) are sufficient to enable power on.
In Auto mode with DETE and CLE = 1, there is no need for a PWON command. The port/channel will automatically attempt to turn on after each detection and classification cycle.
NOTE
In Auto mode, the Power Allocation (0x29h) value needs to be set prior to issuing a PWON command. Any changes to the Power Allocation value after a PWON command is given may be ignored.
A singular PWONn command will be ignored for a 4-Pair wired port in Auto mode.
CLEn | DETEn | Channel Operation | Result of PWONn Command |
---|---|---|---|
0 | 0 | Idle | Singular Turn On attempted with Full DET and CLS cycle |
0 | 1 | Cycling Detection Measurements only | Singular Turn On attempted with Full DET and CLS cycle |
1 | 0 | Idle | Singular Turn On attempted with Full DET and CLS cycle |
1 | 1 | Cycling Detection and Classification Measurements | NA - Channel will power automatically after a valid detection and classification |
PWOFFn in any Mode:
The channel is immediately disabled and the following registers are cleared:
Register | Bits to be Reset |
---|---|
0x04 | CLSCn and DETCn |
0x06 | DISFn and PCUTn |
0x08 | STRTn and ILIMn |
0x0A/B | PCUTnn |
0x0C-0F | Requested Class and Detection |
0x10 | PGn and PEn |
0x14 | CLEn and DETEn |
0x1C | ACn and CCnn |
0x1E-21 | 2P Policing set to 0xFFh |
0x24 | PFn |
0x2A-2B | 4P Policing set to 0xFFh |
0x2D | NLMnn, NCTnn, 4PPCTnn, and DCDTnn |
0x30-3F | Channel Voltage and Current Measurements |
0x40 | 2xFBn |
0x44 - 47 | Detection Resistance Measurements |
0x4C-4F | Assigned Class and Previous Class |
0x51-54 | Autoclass Measurement |
NOTE
It may take upwards of 5ms after PWOFFn command for all register values to be updated.
Only the bits associated with the channel/port ("n") with PWOFFn set will be cleared. Those bits associated with channels/ports remaining in operation will not be changed.
These bits control the response of each channel individually. Thus, it is recommended that for 4-pair wire ports, the bits for both channels be set simultaneously.
NOTE
If only one channel of a 4-pair single signature load with a Class 5 or higher assigned class is given a PWOFFn command, both channels will be disabled.
In the event a singular channel of a 4-pair dual signature PD is turned off due to a PWOFFn command, the power may be reapplied to that channel by setting the PWON bit in 0x19h provided the detection and classification are still valid and the Power Allocation settings in 0x29 are sufficient based on the assigned classification of the powered channel.