JAJS232E November 2006 – October 2019 TPS2410 , TPS2411
PRODUCTION DATA.
PIN | I/O | DESCRIPTION | |
---|---|---|---|
NAME | NO. | ||
VDD | 1 | PWR | Input power for the gate drive charge pump and internal controls. VDD must be connected to a supply voltage ≥ 3 V. |
RSET | 2 | I | Connect a resistor to ground to program the turn-off threshold. Leaving RSET open results in a slightly positive V(A-C) turn-off threshold. |
STAT | 3 | I/O | STAT is a multifunction pin. A high output indicates that the MOSFET gate is being driven high. Overdriving STAT low while GATE is high shifts the fast-turnoff threshold negative. STAT has a weak pull-up to VDD. |
FLTB | 4 | O | Open drain fault output. Fault is active (low) for any of the following conditions:
|
OV | 5 | I | OV is a voltage monitor that contributes to the PG output, and also causes the MOSFET to turn off if it is above the 0.6-V threshold. OV is programmable via an external resistor divider. An OV voltage above 0.6 V indicates a bus voltage that is too high. |
UV | 6 | I | UV is a voltage monitor that contributes to the PG output. The UV input has a 0.6 V threshold and is programmable via an external resistor divider. A UV voltage above 0.6V indicates a bus voltage that is above its minimum acceptable voltage. A low UV input does not effect the gate drive. |
GND | 7 | PWR | Device ground. |
GATE | 8 | O | Connect to the gate of the external MOSFET. Controls the MOSFET to emulate a low forward-voltage diode. |
RSVD | 9 | PWR | This pin must be connected to GND. |
C | 10 | I | Voltage sense input that connects to the simulated diode cathode. Connect to the MOSFET drain in the typical configuration. |
A | 11 | I | Voltage sense input that connects to the simulated diode anode. A also serves as the reference for the charge-pump bias supply on BYP. Connect to the MOSFET source in the typical configuration. |
FLTR | 12 | I | A capacitor connected from FLTR to A filters the input to the fast comparator. Filtering allows the TPS2410 to ignore spurious transients on the A and C inputs. This pin may be left open to achieve the fastest response time. |
BYP | 13 | I/O | Connect a storage capacitor from BYP to A to filter the gate drive supply voltage. |
PG | 14 | O | An open-drain Power Good indicator. PG is open if the UV input is above its threshold, the OV is below its threshold, and the internal UVLO is satisfied. |
PIN | I/O | DESCRIPTION | |
---|---|---|---|
NAME | NO. | ||
BYP | 1 | I/O | Connect a storage capacitor from BYP to A to filter the gate drive supply voltage. |
PG; | 2 | O | An open-drain Power Good indicator. PG is open if the UV input is above its threshold, the OV is below its threshold, and the internal UVLO is satisfied. |
VDD | 3 | PWR | Input power for the gate drive charge pump and internal controls. VDD must be connected to a supply voltage ≥ 3 V. |
RSET | 4 | I | Connect a resistor to ground to program the turn-off threshold. Leaving RSET open results in a slightly positive V(A-C) turn-off threshold. |
STAT | 5 | I/O | STAT is a multifunction pin. A high output indicates that the MOSFET gate is being driven high. Overdriving STAT low while GATE is high shifts the fast-turnoff threshold negative. STAT has a weak pull-up to VDD. |
FLTB | 6 | O | Open drain fault output. Fault is active (low) for any of the following conditions:
|
OV | 7 | I | OV is a voltage monitor that contributes to the PG output, and also causes the MOSFET to turn off if it is above the 0.6-V threshold. OV is programmable via an external resistor divider. An OV voltage above 0.6 V indicates a bus voltage that is too high. |
UV | 8 | I | UV is a voltage monitor that contributes to the PG output. The UV input has a 0.6 V threshold and is programmable via an external resistor divider. A UV voltage above 0.6V indicates a bus voltage that is above its minimum acceptable voltage. A low UV input does not effect the gate drive. |
GND | 9 | PWR | Device ground. |
GATE | 10 | O | Connect to the gate of the external MOSFET. Controls the MOSFET to emulate a low forward-voltage diode. |
RSVD | 11 | PWR | This pin must be connected to GND. |
C | 12 | I | Voltage sense input that connects to the simulated diode cathode. Connect to the MOSFET drain in the typical configuration. |
A | 13 | I | Voltage sense input that connects to the simulated diode anode. A also serves as the reference for the charge-pump bias supply on BYP. Connect to the MOSFET source in the typical configuration. |
FLTR | 14 | I | A capacitor connected from FLTR to A filters the input to the fast comparator. Filtering allows the TPS2410 to ignore spurious transients on the A and C inputs. This pin may be left open to achieve the fastest response time. |