JAJS177F November 2003 – February 2020 TPS2490 , TPS2491
PRODUCTION DATA.
デバイスごとのパッケージ図は、PDF版データシートをご参照ください。
It is critical to select the correct MOSFET for a hot swap design. The device must meet the following requirements:
For this design the CSD19532KTT was selected for its low RDSON and good SOA. After selecting the MOSFET, the maximum steady state case temperature can be computed as follows:
Note that the RDSON is a strong function of junction temperature, which for most MOSFETs will be close to the case temperature. A few iterations of the above equations may be necessary to converge on the final RDSON and TC,MAX value. According to the CSD17552Q5B datasheet, its RDSON is approximately 1.4x at 78°C. The Equation 10 uses this RDSON value to compute the TC,MAX.
This maximum steady state case temperature indicates that a second MOSFET is not needed to reduce and distribute power dissipation during normal operation.
For reference, when using parallel MOSFETs, the maximum steady state case temperature can be computed as follows:
Iterate until the computed TC,MAX is using two parallel MOSFETs is less than to the junction temperature assumed for RDSON. Then, no further iterations are necessary.