JAJSCF6G July 2016 – December 2019 TPS2660
PRODUCTION DATA.
デバイスごとのパッケージ図は、PDF版データシートをご参照ください。
The FLT open-drain output asserts (active low) under following conditions:
The FLT signal can also be used as Power Good indicator to the downstream loads like DC-DC converters. An internal Power Good (PGOOD) signal is OR'd with the fault logic. During start-up, when the device is operating in dVdT mode, PGOOD and FLT remains low and is de-asserted after the dVdT mode is completed and the internal FET is fully enhanced. The PGOOD signal has deglitch time incorporated to ensure that internal FET is fully enhanced before heavy load is applied by the downstream converters. Rising deglitch delay is determined by tPGOOD(degl) = Maximum {(875 + 20 × C(dVdT)), tPGOODR}, where C(dVdT) is in nF and tPGOOD(degl) is in µs. FLT can be left open or connected to RTN when not used. V(IN) falling below V(PORF) = 3.72 V resets FLT.
In case of reverse input polarity fault, care should be taken while interfacing FLT pin to the downstream I/O. Refer to the application report, Fault Handling Using TPS2660 eFuse for further information.