JAJSKH0C April 2023 – February 2024 TPS274C65
PRODUCTION DATA
The current limit thresholds and the inrush current time duration can be set by SPI register writes to enable flexible inrush current control behavior. The following table shows the various options available.
INRUSH_LIMIT[1] |
INRUSH_LIMIT[0] |
Current Limit During Inrush Duration | Notes |
---|---|---|---|
0 |
0 |
Current limit at the
level set by register |
The device will show constant current limit threshold in each channel at all times set by the register values |
0 | 1 | Current limit at 2x the
level set by register |
The current is set higher during the duration of the inrush delay to support high inrush current loads like incandescent lamps - See figure (Case B) showing ex current limit behavior enabling into a short circuit |
1 |
0 |
Current limit at 0.5x
the level set by register |
Feature to limit the current and power dissipation during the charging large power supply capacitor loads. |
1 |
1 |
Current limit fixed at 2.2 A threshold |
An example current limit timing behavior is shown Figure 8-18.
The above waveform shows the current limiting behavior on enabling the outputs during the initial inrush period. The initial inrush current period when the current limit is higher enables two different system advantages when driving loads
While in current limiting mode, at any level, the device will have a high power dissipation. If the FET temperature exceeds the over-temperature shutdown threshold, the device will turn off just the channel that is overloaded. After cooling down, the device will either latch off or re-try, depending on the latch configuration. If the device is turning off prematurely on start-up, it is recommended to improve the PCB thermal layout, lower the current limit to lower power dissipation, or decrease the inrush current (capacitive loading).