JAJSET9B October 2017 – September 2019 TPS27S100
PRODUCTION DATA.
For TPS27S100B, the high-accuracy current-monitor function is internally implemented, which allows a better real-time monitoring effect. A current mirror is used to source 1 / KIMON of the load current, flowing out to the external resistor between the IMON and GND.
KIMON is the ratio of the output current and the sense current. It is a constant value across the temperature and supply voltage range. Each part is factory calibrated during production test, so user-calibration is not required in most cases.
When a fault occurs, the IMON pin also works as a fault report with a pullup voltage, VIMON(H).
Use Equation 1 to calculate RIMON. Also, please ensure VIMON is within the current-sense linear region VIMON(lin) across the full range of the load current.